SAFE.ERROR

Description

Indicates the current error code of the SMM. Possible values of SAFE.ERROR are:

ID

Failure

Comments

0

No fault

 

1

Safe input fault

 

2

SDB failure

 

3

Safe output fault

 

4

STO output fault

 

5

Encoder startup timeout

The communication with the encoder reported a fatal problem. The timeout for the startup of the encoder occurred.

6

Encoder fault: No position available

No encoder position is available but is needed. No valid data is available.

7

Power supply fault (Vcc)

Undervoltage led to a reset of the SMM.

8

Black-channel fault

The safe fieldbus detected a failure.

9..11

Fatal faults

No transmission to drive because there is no active communication.

12

Safety parameter invalid

The drive enters a safe state engaging the brake and removing power simultaneously. This happens when the configured sequence is unknown.

13

Brake output fault

 

14

Temperature fault

The temperature cools when the drive is switched off.

15

Internal discrepancy

A discrepancy between two micro controllers on the SMM was detected.

16

FPGA not suitable

The FPGA software is not suitable for use with this SMM.

17

Internal fault

Error occurred.

18

I/O Fault

Error occurred which can be fixed.

19

Reserved

 

20

External memory fault

A failure occurred at the external non-volatile memory.

21

Manufacturing parameter invalid

The manufacturing data is invalid.

22

External discrepancy

The two inputs used for a dual input are different.

23

Brake current fault

The brake current is out of range.

24

Encoder fault: No speed available

No speed is available but is needed. No valid data is available.

25

Encoder fault:
Invalid association

The association of the encoder to an axis is invalid. No valid data is available.

26

Encoder fault:
Invalid type

The encoder type is invalid. No valid data is available.

27

Encoder fault:
Communication Channel 1

The encoder communication failed on channel 1. No valid data is available.

28

Encoder fault:
Communication Channel 2

The encoder communication failed on channel 2. No valid data is available.

29

Encoder fault:
Communication timeout

The encoder reported a timeout in the communication. No valid data is available.

30

Encoder fault:
Diagnostic test

The encoder reported an error in the diagnostic test. No valid data is available.

31

Encoder fault:
Event Channel 1

The encoder reported an error on channel 1. No valid data is available.

32

Encoder fault:
Event Channel 2

The encoder reported an error on channel 2. No valid data is available.

33

Encoder fault:
Position Drift

The position between channel 1 and 2 is different. No valid data is available.

34

Encoder fault:
Startup error

The encoder reported a failed startup test. No valid data is available.

Code

--> SAFE.ERROR
0

Context

For information on validation refer to Safety Faults, Safety Warnings.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Read Only

Units

N/A

Range

0, 1, 2, 3, 4, 5, 6, 7, 8, 9, 10
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
SAFE.ERROR

37c4h

00h

Unsigned16

-

-

Read only

No